Stock Info
NYSETKR
Recent News
May 20, 2026

The Timken Company (NYSE: TKR; www.timken.com), a leader in advanced motion technology, hosted an Investor Day earlier today in New York City. Lucian Boldea, president and CEO, and other members...

May 8, 2026

The board of directors of The Timken Company (NYSE: TKR; www.timken.com), a global technology leader in engineered bearings and industrial motion, today approved a 2.9 percent increase in the...

May 6, 2026

Sales of $1.23 billion, up 8 percent from last year First-quarter diluted EPS of $1.40; adjusted EPS of $1.67 Net income margin of 8.0 percent; adjusted EBITDA margin of 18.8 percent Raises 2026...

Timken Expands Product Offering of High Performance Spherical Roller Bearings
Bearing Designed to Run Cooler, Longer

NORTH CANTON, Ohio, April 28, 2015 /PRNewswire/ -- The Timken Company (NYSE: TKR; www.timken.com) expects to prompt a spherical revolution with its recent introduction of medium bore high-performance Timken® spherical roller bearings, including new steel cage sizes.

A new line of high-performance Timken(r) spherical roller bearings includes steel cages.

"Customers have made spherical roller bearings an increasingly important element of our core product line. Now they can choose from an even greater selection of sizes featuring steel or brass cages," said Amanda Montgomery, product line vice president for Timken.

Spherical roller bearings are widely used in process industries in equipment ranging from continuous casters, crushers, vibratory screens, excavation loaders and conveyors. To help customers select Timken spherical roller bearings, Timken offers downloads of 2D drawings and 3D models for addition to presentations or insertion directly into a CAD system at www.timken.com/spherical. An interactive catalog with extensive product information and a comprehensive list of spherical roller bearings and accessories also are featured on the website.

Designed to Run Cooler, Longer

In designing the company's high-performance spherical roller bearing offering, Timken engineers added a number of special features that contribute to longer bearing life. Cage pockets, rather than a center guide ring, guide the bearing rollers, thus eliminating a friction point. Based on testing, this design reduces operating temperatures by 5˚C, on average, compared with competitor products.

Testing also showed that eliminating the center guide ring reduces running torque up to 4 percent. Without a guide ring, less friction is created, so less energy is needed to move the bearing and keep it moving, meaning improved efficiency. These features can contribute to longer bearing life, resulting in a product that is designed to:

  • Minimize Wear. Improved profiles designed to reduce internal stresses and optimize load distribution minimize wear.
  • Carry Higher Loads. Longer rollers give more surface area to carry the load, enabling our customers to do more and operate with higher loads.
  • Run Cooler. Enhanced surface finishes can result in improved lube film, which avoids metal-to-metal contact to keep things running cooler.
  • Run Longer. Hardened steel cages are designed to deliver greater fatigue strength, increased wear resistance and tougher protection against shock and acceleration, making it possible for the bearing to run longer.

Learn more about the expanded Timken high-performance spherical roller bearing product line at www.timken.com/spherical.

About The Timken Company

The Timken Company (NYSE: TKR; www.timken.com) engineers, manufactures and markets bearings, transmissions, gearboxes, chain and related products, and offers a spectrum of powertrain rebuild and repair services. The leading authority on tapered roller bearings, Timken today applies its deep knowledge of metallurgy, tribology and mechanical power transmission across a variety of bearings and related systems to improve reliability and efficiency of machinery and equipment all around the world. The company's growing product and services portfolio features many strong industrial brands including Timken®, Fafnir®, Philadelphia Gear® and Drives®. Known for its quality products and collaborative technical sales model, Timken posted $3.1 billion in sales in 2014. With approximately 16,000 people operating from 28 countries, Timken makes the world more productive and keeps industry in motion.

Media Contact:

Investor Contact:

Gloria Irwin

Steve Tschiegg

Communications Manager

Director - Capital Markets & Investor Relations

4500 Mount Pleasant St. N.W.

4500 Mount Pleasant St. N.W.

North Canton, OH 44760 U.S.A.

North Canton, OH 44760 U.S.A.

Telephone: 234.262.3514

Telephone: 234.262.7446

mediarelations@timken.com 

Steve.tschiegg@timken.com

 

The Timken Company Logo

 

Photo - http://photos.prnewswire.com/prnh/20150427/211742

Logo - http://photos.prnewswire.com/prnh/20100210/TIMKENLOGO