Stock Info
NYSETKR
Recent News
May 20, 2026

The Timken Company (NYSE: TKR; www.timken.com), a leader in advanced motion technology, hosted an Investor Day earlier today in New York City. Lucian Boldea, president and CEO, and other members...

May 8, 2026

The board of directors of The Timken Company (NYSE: TKR; www.timken.com), a global technology leader in engineered bearings and industrial motion, today approved a 2.9 percent increase in the...

May 6, 2026

Sales of $1.23 billion, up 8 percent from last year First-quarter diluted EPS of $1.40; adjusted EPS of $1.67 Net income margin of 8.0 percent; adjusted EBITDA margin of 18.8 percent Raises 2026...

Timken Further Expands Round Bar Capabilities
Product Benefits Customers in Industrial, Energy and Bearing Markets

CANTON, Ohio--(BUSINESS WIRE)--March 6, 2007--The Timken Company (NYSE:TKR) today announced that it has further expanded its rolled carbon and alloy steel round bar capabilities and can now produce a maximum diameter of 15 inches. The additional capabilities are the second expansion of the size range in less than a year.


The rolled bar, developed for specific applications, is easier for customers to work with as they manufacture their own products. The new product features a consistent diameter along the full length of the bar, which can significantly improve the cutting of tight mult weights versus using other types of products such as tapered cast ingots. In addition, Timken's large round bars have more hot work than cast ingots, which may allow more flexibility in the size of products that a forger can make.


Rolled bar is used to produce parts for applications such as rolled rings, forgings, gears, bearings and valves for users in the industrial, energy and bearing markets.


Timken is the only domestic U.S. manufacturer to roll 13-, 14- and 15-inch round bars and can produce them in lengths up to 27 feet, 23 feet and 20 feet, respectively. In addition to those capabilities, Timken recently announced a $60 million expansion to enable it to competitively produce small bar steel down to 1 inch in diameter.


"The technological advancements that make this new 15-inch product line possible are part of our strategy to bring new and differentiated product solutions aimed at improving our customers' performance," said Rick Brown, director of advanced product and new business development for Timken's Steel Group. "These larger-diameter, longer bars help reduce handling by our customers and are part of our drive to continually deliver dynamic steel solutions tailored to our customers' growing needs."


About The Timken Company


The Timken Company (NYSE: TKR, www.timken.com) keeps the world turning, with innovative friction management and power transmission products and services, enabling our customers to perform faster and more efficiently. With sales of $5.0 billion in 2006, operations in 26 countries and approximately 25,000 employees, Timken is Where You Turn™ for better performance.


CONTACT: The Timken Company 
Media Contact: Jeff Dafler
Manager - Global Media & Government Relations
Telephone: 330-471-3514
Facsimile: 330-471-7032
jeff.dafler@timken.com
or
Investor Contact: Steve Tschiegg
Manager - Investor Relations
Telephone: 330-471-7446
Facsimile: 330-471-2797
steve.tschiegg@timken.com
or
For Additional Information:
www.timken.com/media
www.timken.com/investors

 

SOURCE: The Timken Company